-(1).png)
Clearing lots or removing trees often means stumps that need to be removed. A stump grinder turns those stumps into chips so you can move on with grading, landscaping, or new construction.
A stump grinder, also known as a stump cutter, is a machine that uses a cutter wheel with carbide teeth to pulverize a stump. Some models resemble a walk‑behind mower; others are larger and ride‑on for higher production.
You position the machine next to the stump, lower the cutter wheel, and move across the wood in controlled passes. Hydraulic cylinders guide the wheel while the teeth shave the stump into chips below ground level.
No. Grinding reduces the stump below grade but leaves the roots in place. Full removal requires digging, severing roots, and extracting the stump. Some teams use a chemical process to accelerate rotting when complete extraction is not practical.
- Walk‑behind: Portable and easy to transport, these machines allow you to handguide the machine during grinding.
- Riding: Compact tractor‑type machines allow you to operate from the seat for longer runs.
- Skid: These track machines grip soft or uneven terrain for better stability.
- Wheeled tow‑behind: These allow you to tow between jobsites for convenient transport.
- Attachment: Work tools mount to larger equipment such as skid steers or backhoe loaders.
Stump grinders are powerful tools. Reduce risk by following these basics:
- Read the operator’s manual and follow the manufacturer’s instructions.
- Call utility locators to verify no buried wires or pipes sit under the stump.
- Inspect and test the machine before work begins.
- Wear a helmet, gloves, boots, earplugs, and safety goggles.
- Avoid loose clothing and secure long hair or accessories.
- Clear rocks, twigs, and other debris from the area.
- Work slowly and keep hands away from moving parts.
Skip grinding if the stump sits next to a building where vibration could affect the foundation. Grinding close to other trees can damage their roots and limit future growth. If the area is inaccessible to machines, chemical removal may be your best option.
You can dispose of chips or use them to backfill the hole and level the ground. Chips also make useful organic mulch at the site or elsewhere. With a heavy volume, some teams resell them.
Yes. If you need the machine only for a project or a season, renting is a convenient, cost‑effective choice. You can select a model that fits your material, site, and budget without long‑term ownership or storage.
Cat Rentals℠ has stump grinder rentals from leading manufacturers at competitive rates. Browse our stump grinder rental inventory today to compare options and availability. To get started, get your quick quote online or find Cat Rentals℠ near you to talk with your local team.