.png)
Effective planning is a core component of any successful construction project. Creating a timeline — a visual display of each step in the process and when it should occur — is an invaluable planning tool. A timeline ensures that everyone knows their role and when they must execute it, which is essential for scheduling. A well-developed timeline can also help prevent cost overruns that can reduce the project's profitability.
While timelines are vital, they can be challenging to create and implement. The following six tips illustrate how to develop a commercial construction project schedule that will lead to the best possible outcome:
Begin by developing a comprehensive schedule in which you break the project down into phases. Start with pre-construction, which includes obtaining permits, preparing contracts and anything else you need to complete before breaking ground. Next steps could include pouring the foundation, framing, HVAC installation and more. Break each phase down into tasks and each task into specific jobs and activities.
Too many project managers focus on finishing the job as quickly as possible to minimize costs and appease the building owners. They may set unrealistic deadlines that lead to inadequate work and costly do-overs. Make sure your plan leaves enough time to complete each project phase without rushing.
No construction project ever goes exactly as planned. Think about all the potential situations that could delay the work (bad weather, labor and material shortages, failure of a subcontractor to perform) and have a contingency plan to manage them.
A commercial construction process is a team effort that requires the successful coordination of architects, subcontractors, builders, HVAC professionals and many others. The more effectively you're able to collaborate and communicate with each partner during planning, the more likely that everyone will stay on the same page as the project unfolds.
The best project managers learn from their mistakes. They keep detailed records as they monitor each project phase. Examine your documentation to determine what worked— and what didn't — on previous jobs. Keep these pitfalls in mind as you plan your future timelines to avoid repeating them.
Periodically review the timeline throughout the project. You may need to make some adjustments in certain areas to keep the work on schedule. You'll also be able to anticipate potential delays and take steps to prevent them.
Effectively planning a project timeline is important, and so is having the right rental equipment for the job. Cat Rentals℠ near you carries bulldozers, excavators, backhoe loaders and anything else you need to keep the work on schedule.
Check out our equipment for rent today. Give us a call at 1-800-RENT-CAT or contact us for a fast quote to get the process started. Rent the high-quality construction machines you need from the experts that do whatever it takes.
To share this page, you are required to accept the use of targeting cookies