.png)
Tilt-up construction has emerged as one of the most widely used building methods in the construction industry. But what exactly does this process entail, and why do so many companies prefer it to other tactics? We'll touch on these topics and more through this comprehensive guide.
Tilt-up construction is the process of raising concrete panels to assemble a building's exterior walls. To accomplish this process, builders must pour concrete into a horizontal floor form and lift the wall out of this mold using a crane. Once the walls assume a vertical position, they are set into foundational footings and braced together until the roof is secure on top.
Tilt-up construction is suitable for residential and commercial projects of all kinds, such as:
- Warehouses
- Manufacturing facilities
- Office buildings
- Retail stores
- Distribution centers
- Schools
- Housing
- Data centers
Tilt-up construction involves more than pouring concrete and lifting walls — this process includes many vital steps to ensure that each panel is solid and secure.
1. Design
Before building the concrete walls, workers must first create a building design that will serve as a framework for the project. The design process involves three primary steps:
- Site assessment: First, the construction team visits the job site to verify that they have complete access to the area and conditions are suitable for concrete building. If so, they can approve the site for construction.
- Planning: The company then designs the building, determining the ideal shape and dimensions. They'll also create a layout outlining how each panel will be arranged before lifting.
- Documentation: Finally, the construction company handles all the necessary paperwork.
2. Construction
One of the most intensive parts of the tilt-up construction process is building the concrete panels that will serve as the walls of the building. Builders create these panels through the following steps:
- Concrete slab construction: To begin, workers pour the concrete slab and install footings at its destination to prepare for panel placement.
- Panel form assembly: Now, the crew can begin creating the panel forms, which serve as wooden molds for the concrete. They'll also install the components and openings needed for features like doors and windows.
- Panel reinforcement: Next, the builders construct a steel grid by tying a series of bars together.
- Insert and embed installation: The team then installs various embeds and inserts, which aid in lifting the panels and attaching them to the roofing, footing and one another.
- Concrete pouring: After confirming there is no debris or standing water on the floor slab, the construction team pours the concrete into the forms to create the panels.
- Insulation: Insulation is applied to each building panel to ensure that the structure is energy-efficient.
3. Lifting
Now that all the necessary pieces have been constructed, it's time to begin raising them into place:
- Form removal: Once the panels solidify, workers remove the forms.
- Crane connecting: The crew then connects the first panel to the crane using cables and a hook that attaches to the inserts.
- Panel placement: After the workers attach braces to the panel, they use the crane to lift it from the floor slab to a vertical position over the footings. They then position the panel and set it in place.
- Panel securing: To attach the panel, the team connects the panel's braces to the slab and its embeds to the footing before disconnecting the crane cables.
- Repeat: The crew repeats this process for each panel until all of them are level, straight and secure.
- Finishing: The builders add the finishing touches to the building, such as paint, sandblasting, stains, caulk and patches.
- Roofing: Finally, the building's roof is installed.
Tilt-up construction is among the most popular commercial construction methods in the country due to its many groundbreaking advantages:
- Cost-efficiency: Tilt-up walls require fewer crew members and machinery to assemble compared to other building methods, minimizing labor and equipment costs.
- Installation speed: Erecting a building through tilt-up construction takes significantly less time to complete than other methods, and it allows for a highly efficient design/build process.
- Design flexibility: Tilt-up buildings have many design and aesthetic possibilities, from building finishes to wall textures to embellishments.
- Energy-efficiency: Because tilt-up buildings comprise concrete and built-in insulation, they promote energy savings.
- Durability: Buildings produced from tilt-up construction methods are designed to stand the test of time, showing little signs of aging even 50 years after assembly. These structures are also fire-resistant.
If you require heavy equipment for your next tilt-up construction project, you can rent what you need at Cat Rentals℠. We provide our customers with reliable and cost-effective equipment at the most flexible rental terms.
Call 1-800-RENT-CAT to learn more about our products or browse our equipment online!