.png)
Underground pipes are common in farming, drainage, and residential projects. They reduce water pooling, look cleaner than above-ground pipes, and add value to property. To install them safely and on time, you’ll need the right equipment. Here are the basic tools for underground pipe installation.
Excavator
An excavator prepares the site. It clears brush and debris and digs the trench. Tracked excavators work well on rough ground. Mini excavators are best in small spaces. After the pipes are laid, use the excavator to backfill the trench.
Trencher
A trencher digs the trench where the pipes will go. Its fast-moving chain with sharp teeth cuts through soil and rock. Choose tracked or wheeled models depending on the ground conditions.
Trench Shoring
Trench shoring is safety gear. It keeps trench walls from caving in and protects workers. Different styles are available to match trench size and soil type.
Pipe Laser
A pipe laser helps ensure the trench is dug to the correct slope so water flows smoothly through the pipe. This prevents dips or rises that could cause blockages.
Pipelayer
A pipelayer places the pipes in the trench. Some models can lift pipes weighing over 200,000 pounds. Tracks allow them to stay stable even on uneven ground.
Compactor
Once pipes are in place, the soil must be packed tight. A compactor presses the soil down to remove air pockets and prevent settling. Different compactors are available for different soil types and project sizes.
Rent Pipe Installation Tools From Cat Rentals℠
Cat Rentals has the machines you need for underground pipe installation — from excavators to compactors. We offer flexible rental terms and dependable dealer support. Browse our equipment or find your local dealer to request a quote today.
FAQs About Underground Pipe Installation Tools
What tool is most important for underground pipe installation?
Excavators and trenchers are the main tools for site prep and digging.
Why use trench shoring?
It prevents trench walls from collapsing and keeps workers safe.
Can I rent all of these tools?
Yes. Cat Rentals rents excavators, trenchers, pipelayers, compactors, and more.