Should I Use a Utility Trailer When Moving?
When planning a move, one of the first questions is how you’ll transport your belongings. Most people consider renting a moving truck, but that’s not the only option. A utility trailer may be a better fit depending on the size, distance and type of items you’re moving. This guide explains the pros and cons of using a utility trailer so you can decide what works best for your move.
What Are Your Options for Moving?
The two most common moving vehicle options are moving trucks and utility trailers. A moving truck is self-contained and usually large enough to fit all your belongings at once. A trailer, by contrast, attaches to a pickup or SUV and provides extra hauling space. Each option has benefits depending on your needs.
What Is a Utility Trailer?
A utility trailer is an open or enclosed platform on wheels that attaches to a towing vehicle. They come in many sizes, from small single-axle units for light loads to large dual-axle trailers for heavier equipment.
You can haul items such as:
- Furniture and appliances
- Moving boxes and totes
- Yard equipment like mowers or ATVs
- Construction or landscaping materials
Because trailers are versatile, they’re useful not just for moving household items but also for projects before or after your move, like hauling debris, tools, or supplies.
Utility Trailer vs. Moving Truck
Here’s how the two options compare:
- Cost: Utility trailers usually cost less to rent than moving trucks, especially for local moves where you already have a towing vehicle.
- Capacity: Moving trucks can fit an entire household in one trip. Trailers may require multiple trips depending on load size.
- Convenience: With a trailer, you can use your own vehicle, avoid learning to drive a large truck, and keep passengers or pets with you during the move.
- Fuel efficiency: Towing a trailer often uses less fuel than renting and driving a moving truck, particularly for shorter moves.
If you’re moving across town or only transporting part of your belongings, a utility trailer may be the simplest and most affordable option. For long-distance or full-household moves, a moving truck could save time by reducing the number of trips.
When Should You Use Both a Trailer and a Truck?
In some cases, combining both options makes sense. For example, if you need a truck for furniture but also want extra space for yard tools or fragile items, a trailer provides overflow capacity. Contractors or DIY movers often rent both when relocating tools and household items at the same time.
Tips for Safe Trailer Use
If you decide on a utility trailer, keep these safety tips in mind:
- Check that your vehicle is rated to tow the trailer’s weight.
- Balance loads evenly and secure items with straps or tie-downs.
- Double-check trailer lights and brakes before hitting the road.
- Drive slower than usual, leaving extra room for braking and turning.
Rent Utility Trailers at Cat Rentals℠
Cat Rentals℠ offers a wide range of utility trailers to make moving easier. You can browse rental trailers or find the Cat Rentals near you to connect with your local dealer today.
Find Cat Rentals Near You